ABB Ability™ History UI SDK - Client API Reference
    Preparing search index...

    The base for all standard value accessors

    Hierarchy (View Summary)

    Implements

    Index

    Constructors

    Properties

    AutoScaling: IProperty<boolean> = ...

    Have the widget to set the scale automatically according the incoming values. (Only supported by certain accessors.)

    AutoScalingMode: IProperty<AutoScaleMode> = ...

    The type of auto scaling used.

    Changed: IEvent<void> = ...

    Fired when the data of the value accessor has changed.

    Connection: IConnectionAPI

    The connection API for the value accessor

    Context: IContextAPI = ...

    The context handling API for the value accessor

    CustomDescription: IProperty<string> = ...

    The user-definable description that overrides any defaults.

    CustomMaximumValue: IProperty<number> = ...

    The user-definable minimum value that overrides any defaults.

    CustomMinimumValue: IProperty<number> = ...

    The user-definable minimum value that overrides any defaults.

    CustomName: IProperty<string> = ...

    The user-definable name that overrides any defaults.

    CustomUnit: IProperty<string> = ...

    The user-definable unit that overrides any defaults.

    DefaultStorage: IDefaultStorage = ...

    Default property value storage - used by the default property getters and setters.

    Description: IProperty<string> = ...

    The description shown to user. (Automatically fetched)

    DisplayName: IProperty<string> = ...

    The display name shown to user.

    DisposeEvent: IManualEvent<void>

    Dispose Event signaled when the object is being disposed. NOTE: Inheriting classes should use AddDisposeHandler instead.

    Events: IEvents

    cClassBase event API

    Initialized: IManualEvent<void> = ...

    Fired when the value accessor has been initialized.

    InitializeFailed: IManualEvent<void> = ...

    Fired when the value accessor initialization has failed.

    MaximumValue: IProperty<unknown> = ...

    The default maximum value. (Automatically fetched)

    MinimumValue: IProperty<unknown> = ...

    The default minimum value. (Automatically fetched)

    PathName: IProperty<string> = ...

    Process path that may be shown in the tooltip

    TooltipDecimals: IProperty<number> = ...

    Max. Number of decimals shown in the tooltip

    UId: IProperty<string>
    Unit: IProperty<string> = ...

    The default unit. (Automatically fetched)

    Accessors

    • get CanDispose(): boolean

      The object can be disposed

      Returns boolean

    • set CanDispose(value: boolean): void

      Parameters

      • value: boolean

      Returns void

    • get NLS(): IComponentNLSRequest

      The component class specific NLS request

      Returns IComponentNLSRequest

    • get Properties(): IPropertyAPI

      The component property API

      Returns IPropertyAPI

    Methods

    • Returns ILegacyBase

    • Create function that can abort asynchronous code in case the function is called again or the owner instance have been disposed. This is useful with problematic cases where for example server request is sent and the return is handled asynchronously (with a callback). Meanwhile the configuration may have changed making the code in the callback unnecessary or even harmful. *

      Type Parameters

      • TArgs extends unknown[] = []

      Parameters

      • func: TAsyncAbortable<TArgs>

        A function with first parameter as function to check the abort state: Can be used in the function: if(abort()) return; //abort

      • disposeonly: boolean = false

        Check only the dispose state - don't check subsequent calls to the function.

      Returns TAsyncAbortableReturn<TArgs>

    • Add a dispose handler called when this object is being disposed. The dispose handlers are called in reverse order (the latest first).

      Parameters

      • disposer: () => void

        The dispose handler - should make any manual clean up necessary when the object is being disposed.

      Returns void

    • Get the value of a named property.

      Type Parameters

      • T

      Parameters

      • propertyname: string

        The name of the property

      Returns T

    • Accessor has benn initialized.

      Returns boolean

    • Set a value for the named property.

      Type Parameters

      • T

      Parameters

      • propertyname: string

        The name of the property

      • value: T

        The new value for the property

      Returns void

    • String representation of the component instance. Can be overridden by inheriting classes.

      Returns string