ABB Ability™ History UI SDK - Client API Reference
    Preparing search index...

    Type Alias TGetStandardValuesResult

    GetStandardValues Result

    type TGetStandardValuesResult = {
        Exclusive: boolean;
        Flags: boolean;
        RawType: string;
        RawValue: unknown;
        Supported: boolean;
        Truncated: boolean;
        Type: string;
        Values: TStandardValuesItem[];
    }
    Index

    Properties

    Exclusive: boolean

    Only returned values supported

    Flags: boolean

    Values are flags (bits or bit fields that can be combined by bitwise operation)

    RawType: string

    Raw type of the property

    RawValue: unknown

    The user input as Raw value

    Supported: boolean

    Standard values for the property are supported

    Truncated: boolean

    Fetch limit reached - some options were not included

    Type: string

    Property Type

    Value options for the property