cMessage |
The cMessageBox type exposes the following members.
| Name | Description | |
|---|---|---|
| Activate | Activates the form and gives it focus. (Inherited from Form) | |
| AddOwnedForm | Adds an owned form to this form. (Inherited from Form) | |
| BeginInvoke(Delegate) | Executes the specified delegate asynchronously on the thread that the control's underlying handle was created on. (Inherited from Control) | |
| BeginInvoke(Delegate, Object) | Executes the specified delegate asynchronously with the specified arguments, on the thread that the control's underlying handle was created on. (Inherited from Control) | |
| BringToFront | Brings the control to the front of the z-order. (Inherited from Control) | |
| Close | Closes the form. (Inherited from Form) | |
| Contains | Retrieves a value indicating whether the specified control is a child of the control. (Inherited from Control) | |
| CreateControl | Forces the creation of the visible control, including the creation of the handle and any visible child controls. (Inherited from Control) | |
| CreateGraphics | Creates the Graphics for the control. (Inherited from Control) | |
| CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from MarshalByRefObject) | |
| Dispose | Releases all resources used by the Component. (Inherited from Component) | |
| DoDragDrop | Begins a drag-and-drop operation. (Inherited from Control) | |
| DrawToBitmap | Supports rendering to the specified bitmap. (Inherited from Control) | |
| EndInvoke | Retrieves the return value of the asynchronous operation represented by the IAsyncResult passed. (Inherited from Control) | |
| Equals | Determines whether the specified object is equal to the current object. (Inherited from Object) | |
| FindForm | Retrieves the form that the control is on. (Inherited from Control) | |
| Focus | Sets input focus to the control. (Inherited from Control) | |
| GetChildAtPoint(Point) | Retrieves the child control that is located at the specified coordinates. (Inherited from Control) | |
| GetChildAtPoint(Point, GetChildAtPointSkip) | Retrieves the child control that is located at the specified coordinates, specifying whether to ignore child controls of a certain type. (Inherited from Control) | |
| GetContainerControl | Returns the next ContainerControl up the control's chain of parent controls. (Inherited from Control) | |
| GetHashCode | Serves as the default hash function. (Inherited from Object) | |
| GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from MarshalByRefObject) | |
| GetNextControl | Retrieves the next control forward or back in the tab order of child controls. (Inherited from Control) | |
| GetPreferredSize | Retrieves the size of a rectangular area into which a control can be fitted. (Inherited from Control) | |
| GetType | Gets the Type of the current instance. (Inherited from Object) | |
| Hide | Conceals the control from the user. (Inherited from Control) | |
| InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from MarshalByRefObject) | |
| Invalidate | Invalidates the entire surface of the control and causes the control to be redrawn. (Inherited from Control) | |
| Invalidate(Boolean) | Invalidates a specific region of the control and causes a paint message to be sent to the control. Optionally, invalidates the child controls assigned to the control. (Inherited from Control) | |
| Invalidate(Rectangle) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. (Inherited from Control) | |
| Invalidate(Region) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. (Inherited from Control) | |
| Invalidate(Rectangle, Boolean) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. Optionally, invalidates the child controls assigned to the control. (Inherited from Control) | |
| Invalidate(Region, Boolean) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. Optionally, invalidates the child controls assigned to the control. (Inherited from Control) | |
| Invoke(Delegate) | Executes the specified delegate on the thread that owns the control's underlying window handle. (Inherited from Control) | |
| Invoke(Delegate, Object) | Executes the specified delegate, on the thread that owns the control's underlying window handle, with the specified list of arguments. (Inherited from Control) | |
| LayoutMdi | Arranges the multiple-document interface (MDI) child forms within the MDI parent form. (Inherited from Form) | |
| LogicalToDeviceUnits | Converts a Logical DPI value to it's equivalent DeviceUnit DPI value. (Inherited from Control) | |
| PerformAutoScale | Performs scaling of the container control and its children. (Inherited from ContainerControl) | |
| PerformLayout | Forces the control to apply layout logic to all its child controls. (Inherited from Control) | |
| PerformLayout(Control, String) | Forces the control to apply layout logic to all its child controls. (Inherited from Control) | |
| PointToClient | Computes the location of the specified screen point into client coordinates. (Inherited from Control) | |
| PointToScreen | Computes the location of the specified client point into screen coordinates. (Inherited from Control) | |
| PreProcessControlMessage | Preprocesses keyboard or input messages within the message loop before they are dispatched. (Inherited from Control) | |
| PreProcessMessage | Preprocesses keyboard or input messages within the message loop before they are dispatched. (Inherited from Control) | |
| RectangleToClient | Computes the size and location of the specified screen rectangle in client coordinates. (Inherited from Control) | |
| RectangleToScreen | Computes the size and location of the specified client rectangle in screen coordinates. (Inherited from Control) | |
| Refresh | Forces the control to invalidate its client area and immediately redraw itself and any child controls. (Inherited from Control) | |
| RemoveOwnedForm | Removes an owned form from this form. (Inherited from Form) | |
| ResetBackColor | Resets the BackColor property to its default value. (Inherited from Control) | |
| ResetBindings | Causes a control bound to the BindingSource to reread all the items in the list and refresh their displayed values. (Inherited from Control) | |
| ResetCursor | Resets the Cursor property to its default value. (Inherited from Control) | |
| ResetFont | Resets the Font property to its default value. (Inherited from Control) | |
| ResetForeColor | Resets the ForeColor property to its default value. (Inherited from Control) | |
| ResetImeMode | Resets the ImeMode property to its default value. (Inherited from Control) | |
| ResetRightToLeft | Resets the RightToLeft property to its default value. (Inherited from Control) | |
| ResetText | Resets the Text property to its default value. (Inherited from Control) | |
| ResumeLayout | Resumes usual layout logic. (Inherited from Control) | |
| ResumeLayout(Boolean) | Resumes usual layout logic, optionally forcing an immediate layout of pending layout requests. (Inherited from Control) | |
| Scale(Single) | Obsolete. Scales the control and any child controls. (Inherited from Control) | |
| Scale(SizeF) | Scales the control and all child controls by the specified scaling factor. (Inherited from Control) | |
| Scale(Single, Single) | Obsolete. Scales the entire control and any child controls. (Inherited from Control) | |
| ScaleBitmapLogicalToDevice | Scales a logical bitmap value to it's equivalent device unit value when a DPI change occurs. (Inherited from Control) | |
| ScrollControlIntoView | Scrolls the specified child control into view on an auto-scroll enabled control. (Inherited from ScrollableControl) | |
| Select | Activates the control. (Inherited from Control) | |
| SelectNextControl | Activates the next control. (Inherited from Control) | |
| SendToBack | Sends the control to the back of the z-order. (Inherited from Control) | |
| SetAutoScrollMargin | Sets the size of the auto-scroll margins. (Inherited from ScrollableControl) | |
| SetBounds(Int32, Int32, Int32, Int32) | Sets the bounds of the control to the specified location and size. (Inherited from Control) | |
| SetBounds(Int32, Int32, Int32, Int32, BoundsSpecified) | Sets the specified bounds of the control to the specified location and size. (Inherited from Control) | |
| SetDesktopBounds | Sets the bounds of the form in desktop coordinates. (Inherited from Form) | |
| SetDesktopLocation | Sets the location of the form in desktop coordinates. (Inherited from Form) | |
| Show | Displays the control to the user. (Inherited from Control) | |
| Show(IWin32Window) | Shows the form with the specified owner to the user. (Inherited from Form) | |
| Show(Object, String, String, cMessageBoxButtons, cMessageBoxIcon) | ||
| Show(Object, String, String, cMessageBoxButtons, cMessageBoxIcon, cMessageBoxDefaultButton) | ||
| Show(Object, String, String, String, cMessageBoxIcon, Int32) | ||
| Show(Object, String, String, String, cMessageBoxIcon, Int32, Int32) | ||
| ShowBox | ||
| ShowDialog | Shows the form as a modal dialog box. (Inherited from Form) | |
| ShowDialog(IWin32Window) | Shows the form as a modal dialog box with the specified owner. (Inherited from Form) | |
| SuspendLayout | Temporarily suspends the layout logic for the control. (Inherited from Control) | |
| ToString | Gets a string representing the current instance of the form. (Inherited from Form) | |
| Update | Causes the control to redraw the invalidated regions within its client area. (Inherited from Control) | |
| Validate | Verifies the value of the control losing focus by causing the Validating and Validated events to occur, in that order. (Inherited from ContainerControl) | |
| Validate(Boolean) | Verifies the value of the control that is losing focus; conditionally dependent on whether automatic validation is turned on. (Inherited from ContainerControl) | |
| ValidateChildren | Causes all of the child controls within a control that support validation to validate their data. (Inherited from Form) | |
| ValidateChildren(ValidationConstraints) | Causes all of the child controls within a control that support validation to validate their data. (Inherited from Form) |