cMessage |
The cMessageBox type exposes the following members.
| Name | Description | |
|---|---|---|
| AcceptButton | Gets or sets the button on the form that is clicked when the user presses the ENTER key. (Inherited from Form) | |
| AccessibilityObject | Gets the AccessibleObject assigned to the control. (Inherited from Control) | |
| AccessibleDefaultActionDescription | Gets or sets the default action description of the control for use by accessibility client applications. (Inherited from Control) | |
| AccessibleDescription | Gets or sets the description of the control used by accessibility client applications. (Inherited from Control) | |
| AccessibleName | Gets or sets the name of the control used by accessibility client applications. (Inherited from Control) | |
| AccessibleRole | Gets or sets the accessible role of the control (Inherited from Control) | |
| ActiveControl | Gets or sets the active control on the container control. (Inherited from ContainerControl) | |
| ActiveMdiChild | Gets the currently active multiple-document interface (MDI) child window. (Inherited from Form) | |
| AllowDrop | Gets or sets a value indicating whether the control can accept data that the user drags onto it. (Inherited from Control) | |
| AllowTransparency | Gets or sets a value indicating whether the opacity of the form can be adjusted. (Inherited from Form) | |
| Anchor | Gets or sets the edges of the container to which a control is bound and determines how a control is resized with its parent. (Inherited from Control) | |
| AutoScale | Obsolete. Gets or sets a value indicating whether the form adjusts its size to fit the height of the font used on the form and scales its controls. (Inherited from Form) | |
| AutoScaleBaseSize | Gets or sets the base size used for autoscaling of the form. (Inherited from Form) | |
| AutoScaleDimensions | Gets or sets the dimensions that the control was designed to. (Inherited from ContainerControl) | |
| AutoScaleMode | Gets or sets the automatic scaling mode of the control. (Inherited from ContainerControl) | |
| AutoScroll | Gets or sets a value indicating whether the form enables autoscrolling. (Inherited from Form) | |
| AutoScrollMargin | Gets or sets the size of the auto-scroll margin. (Inherited from ScrollableControl) | |
| AutoScrollMinSize | Gets or sets the minimum size of the auto-scroll. (Inherited from ScrollableControl) | |
| AutoScrollOffset | Gets or sets where this control is scrolled to in ScrollControlIntoView(Control). (Inherited from Control) | |
| AutoScrollPosition | Gets or sets the location of the auto-scroll position. (Inherited from ScrollableControl) | |
| AutoSize | Resize the form according to the setting of AutoSizeMode. (Inherited from Form) | |
| AutoSizeMode | Gets or sets the mode by which the form automatically resizes itself. (Inherited from Form) | |
| AutoValidate | Gets or sets a value that indicates whether controls in this container will be automatically validated when the focus changes. (Inherited from Form) | |
| BackColor | Gets or sets the background color for the control. (Inherited from Form) | |
| BackgroundImage | Gets or sets the background image displayed in the control. (Inherited from Control) | |
| BackgroundImageLayout | Gets or sets the background image layout as defined in the ImageLayout enumeration. (Inherited from Control) | |
| BindingContext | Gets or sets the BindingContext for the control. (Inherited from ContainerControl) | |
| Bottom | Gets the distance, in pixels, between the bottom edge of the control and the top edge of its container's client area. (Inherited from Control) | |
| Bounds | Gets or sets the size and location of the control including its nonclient elements, in pixels, relative to the parent control. (Inherited from Control) | |
| CancelButton | Gets or sets the button control that is clicked when the user presses the ESC key. (Inherited from Form) | |
| CanFocus | Gets a value indicating whether the control can receive focus. (Inherited from Control) | |
| CanSelect | Gets a value indicating whether the control can be selected. (Inherited from Control) | |
| Capture | Gets or sets a value indicating whether the control has captured the mouse. (Inherited from Control) | |
| CausesValidation | Gets or sets a value indicating whether the control causes validation to be performed on any controls that require validation when it receives focus. (Inherited from Control) | |
| ClientRectangle | Gets the rectangle that represents the client area of the control. (Inherited from Control) | |
| ClientSize | Gets or sets the size of the client area of the form. (Inherited from Form) | |
| CompanyName | Gets the name of the company or creator of the application containing the control. (Inherited from Control) | |
| Container | Gets the IContainer that contains the Component. (Inherited from Component) | |
| ContainsFocus | Gets a value indicating whether the control, or one of its child controls, currently has the input focus. (Inherited from Control) | |
| ContextMenu | Gets or sets the shortcut menu associated with the control. (Inherited from Control) | |
| ContextMenuStrip | Gets or sets the ContextMenuStrip associated with this control. (Inherited from Control) | |
| ControlBox | Gets or sets a value indicating whether a control box is displayed in the caption bar of the form. (Inherited from Form) | |
| Controls | Gets the collection of controls contained within the control. (Inherited from Control) | |
| Created | Gets a value indicating whether the control has been created. (Inherited from Control) | |
| CurrentAutoScaleDimensions | Gets the current run-time dimensions of the screen. (Inherited from ContainerControl) | |
| Cursor | Gets or sets the cursor that is displayed when the mouse pointer is over the control. (Inherited from Control) | |
| DataBindings | Gets the data bindings for the control. (Inherited from Control) | |
| DesktopBounds | Gets or sets the size and location of the form on the Windows desktop. (Inherited from Form) | |
| DesktopLocation | Gets or sets the location of the form on the Windows desktop. (Inherited from Form) | |
| DeviceDpi | Gets the DPI value for the display device where the control is currently being displayed. (Inherited from Control) | |
| DialogResult | Gets or sets the dialog result for the form. (Inherited from Form) | |
| DisplayRectangle | Gets the rectangle that represents the virtual display area of the control. (Inherited from ScrollableControl) | |
| Disposing | Gets a value indicating whether the base Control class is in the process of disposing. (Inherited from Control) | |
| Dock | Gets or sets which control borders are docked to its parent control and determines how a control is resized with its parent. (Inherited from Control) | |
| DockPadding | Gets the dock padding settings for all edges of the control. (Inherited from ScrollableControl) | |
| Enabled | Gets or sets a value indicating whether the control can respond to user interaction. (Inherited from Control) | |
| Focused | Gets a value indicating whether the control has input focus. (Inherited from Control) | |
| Font | Gets or sets the font of the text displayed by the control. (Inherited from Control) | |
| ForeColor | Gets or sets the foreground color of the control. (Inherited from Control) | |
| FormBorderStyle | Gets or sets the border style of the form. (Inherited from Form) | |
| Handle | Gets the window handle that the control is bound to. (Inherited from Control) | |
| HasChildren | Gets a value indicating whether the control contains one or more child controls. (Inherited from Control) | |
| Height | Gets or sets the height of the control. (Inherited from Control) | |
| HelpButton | Gets or sets a value indicating whether a Help button should be displayed in the caption box of the form. (Inherited from Form) | |
| HorizontalScroll | Gets the characteristics associated with the horizontal scroll bar. (Inherited from ScrollableControl) | |
| Icon | Gets or sets the icon for the form. (Inherited from Form) | |
| ImeMode | Gets or sets the Input Method Editor (IME) mode of the control. (Inherited from Control) | |
| InvokeRequired | Gets a value indicating whether the caller must call an invoke method when making method calls to the control because the caller is on a different thread than the one the control was created on. (Inherited from Control) | |
| IsAccessible | Gets or sets a value indicating whether the control is visible to accessibility applications. (Inherited from Control) | |
| IsDisposed | Gets a value indicating whether the control has been disposed of. (Inherited from Control) | |
| IsHandleCreated | Gets a value indicating whether the control has a handle associated with it. (Inherited from Control) | |
| IsMdiChild | Gets a value indicating whether the form is a multiple-document interface (MDI) child form. (Inherited from Form) | |
| IsMdiContainer | Gets or sets a value indicating whether the form is a container for multiple-document interface (MDI) child forms. (Inherited from Form) | |
| IsMirrored | Gets a value indicating whether the control is mirrored. (Inherited from Control) | |
| IsRestrictedWindow | Gets a value indicating whether the form can use all windows and user input events without restriction. (Inherited from Form) | |
| KeyPreview | Gets or sets a value indicating whether the form will receive key events before the event is passed to the control that has focus. (Inherited from Form) | |
| LayoutEngine | Gets a cached instance of the control's layout engine. (Inherited from Control) | |
| Left | Gets or sets the distance, in pixels, between the left edge of the control and the left edge of its container's client area. (Inherited from Control) | |
| Location | Gets or sets the Point that represents the upper-left corner of the Form in screen coordinates. (Inherited from Form) | |
| MainMenuStrip | Gets or sets the primary menu container for the form. (Inherited from Form) | |
| Margin | Gets or sets the space between controls. (Inherited from Form) | |
| MaximizeBox | Gets or sets a value indicating whether the Maximize button is displayed in the caption bar of the form. (Inherited from Form) | |
| MaximumSize | Gets the maximum size the form can be resized to. (Inherited from Form) | |
| MdiChildren | Gets an array of forms that represent the multiple-document interface (MDI) child forms that are parented to this form. (Inherited from Form) | |
| MdiParent | Gets or sets the current multiple-document interface (MDI) parent form of this form. (Inherited from Form) | |
| Menu | Gets or sets the MainMenu that is displayed in the form. (Inherited from Form) | |
| MergedMenu | Gets the merged menu for the form. (Inherited from Form) | |
| MinimizeBox | Gets or sets a value indicating whether the Minimize button is displayed in the caption bar of the form. (Inherited from Form) | |
| MinimumSize | Gets or sets the minimum size the form can be resized to. (Inherited from Form) | |
| Modal | Gets a value indicating whether this form is displayed modally. (Inherited from Form) | |
| Name | Gets or sets the name of the control. (Inherited from Control) | |
| Opacity | Gets or sets the opacity level of the form. (Inherited from Form) | |
| OwnedForms | Gets an array of Form objects that represent all forms that are owned by this form. (Inherited from Form) | |
| Owner | Gets or sets the form that owns this form. (Inherited from Form) | |
| Padding | Gets or sets padding within the control. (Inherited from Control) | |
| Parent | Gets or sets the parent container of the control. (Inherited from Control) | |
| ParentForm | Gets the form that the container control is assigned to. (Inherited from ContainerControl) | |
| PreferredSize | Gets the size of a rectangular area into which the control can fit. (Inherited from Control) | |
| ProductName | Gets the product name of the assembly containing the control. (Inherited from Control) | |
| ProductVersion | Gets the version of the assembly containing the control. (Inherited from Control) | |
| RecreatingHandle | Gets a value indicating whether the control is currently re-creating its handle. (Inherited from Control) | |
| Region | Gets or sets the window region associated with the control. (Inherited from Control) | |
| RestoreBounds | Gets the location and size of the form in its normal window state. (Inherited from Form) | |
| ReturnValue | ||
| Right | Gets the distance, in pixels, between the right edge of the control and the left edge of its container's client area. (Inherited from Control) | |
| RightToLeft | Gets or sets a value indicating whether control's elements are aligned to support locales using right-to-left fonts. (Inherited from Control) | |
| RightToLeftLayout | Gets or sets a value indicating whether right-to-left mirror placement is turned on. (Inherited from Form) | |
| ShowIcon | Gets or sets a value indicating whether an icon is displayed in the caption bar of the form. (Inherited from Form) | |
| ShowInTaskbar | Gets or sets a value indicating whether the form is displayed in the Windows taskbar. (Inherited from Form) | |
| Site | Gets or sets the site of the control. (Inherited from Control) | |
| Size | Gets or sets the size of the form. (Inherited from Form) | |
| SizeGripStyle | Gets or sets the style of the size grip to display in the lower-right corner of the form. (Inherited from Form) | |
| StartPosition | Gets or sets the starting position of the form at run time. (Inherited from Form) | |
| TabIndex | Gets or sets the tab order of the control within its container. (Inherited from Form) | |
| TabStop | Gets or sets a value indicating whether the user can give the focus to this control using the TAB key. (Inherited from Form) | |
| Tag | Gets or sets the object that contains data about the control. (Inherited from Control) | |
| Text | Gets or sets the text associated with this control. (Inherited from Form) | |
| Top | Gets or sets the distance, in pixels, between the top edge of the control and the top edge of its container's client area. (Inherited from Control) | |
| TopLevel | Gets or sets a value indicating whether to display the form as a top-level window. (Inherited from Form) | |
| TopLevelControl | Gets the parent control that is not parented by another Windows Forms control. Typically, this is the outermost Form that the control is contained in. (Inherited from Control) | |
| TopMost | Gets or sets a value indicating whether the form should be displayed as a topmost form. (Inherited from Form) | |
| TransparencyKey | Gets or sets the color that will represent transparent areas of the form. (Inherited from Form) | |
| UseWaitCursor | Gets or sets a value indicating whether to use the wait cursor for the current control and all child controls. (Inherited from Control) | |
| VerticalScroll | Gets the characteristics associated with the vertical scroll bar. (Inherited from ScrollableControl) | |
| Visible | Gets or sets a value indicating whether the control and all its child controls are displayed. (Inherited from Control) | |
| Width | Gets or sets the width of the control. (Inherited from Control) | |
| WindowState | Gets or sets a value that indicates whether form is minimized, maximized, or normal. (Inherited from Form) | |
| WindowTarget | This property is not relevant for this class. (Inherited from Control) |