Click or drag to resize

cDbClassInstancecUpdateInfo Class

[Missing <summary> documentation for "T:ABB.Vtrin.cDbClassInstance.cUpdateInfo"]

Inheritance Hierarchy
SystemObject
  ABB.VtrincDbClassInstancecUpdateInfo

Namespace: ABB.Vtrin
Assembly: VtrinLib (in VtrinLib.dll) Version: 530.2607.2220.0 (RTDB_main)
Syntax
protected internal class cUpdateInfo

The cDbClassInstancecUpdateInfo type exposes the following members.

Constructors
 NameDescription
Public methodcDbClassInstancecUpdateInfoInitializes a new instance of the cDbClassInstancecUpdateInfo class
Top
Methods
 NameDescription
Public methodEqualsDetermines whether the specified object is equal to the current object.
(Inherited from Object)
Protected methodFinalizeAllows an object to try to free resources and perform other cleanup operations before it is reclaimed by garbage collection.
(Inherited from Object)
Public methodGetHashCodeServes as the default hash function.
(Inherited from Object)
Public methodGetTypeGets the Type of the current instance.
(Inherited from Object)
Protected methodMemberwiseCloneCreates a shallow copy of the current Object.
(Inherited from Object)
Public methodToStringReturns a string that represents the current object.
(Inherited from Object)
Top
Fields
See Also