cMessage |
[Missing <summary> documentation for "T:ABB.Vtrin.cMessageBox"]
The cMessageBox type exposes the following members.
| Name | Description | |
|---|---|---|
| AcceptButton | Gets or sets the button on the form that is clicked when the user presses the ENTER key. (Inherited from Form) | |
| AccessibilityObject | Gets the AccessibleObject assigned to the control. (Inherited from Control) | |
| AccessibleDefaultActionDescription | Gets or sets the default action description of the control for use by accessibility client applications. (Inherited from Control) | |
| AccessibleDescription | Gets or sets the description of the control used by accessibility client applications. (Inherited from Control) | |
| AccessibleName | Gets or sets the name of the control used by accessibility client applications. (Inherited from Control) | |
| AccessibleRole | Gets or sets the accessible role of the control (Inherited from Control) | |
| ActiveControl | Gets or sets the active control on the container control. (Inherited from ContainerControl) | |
| ActiveMdiChild | Gets the currently active multiple-document interface (MDI) child window. (Inherited from Form) | |
| AllowDrop | Gets or sets a value indicating whether the control can accept data that the user drags onto it. (Inherited from Control) | |
| AllowTransparency | Gets or sets a value indicating whether the opacity of the form can be adjusted. (Inherited from Form) | |
| Anchor | Gets or sets the edges of the container to which a control is bound and determines how a control is resized with its parent. (Inherited from Control) | |
| AutoScale | Obsolete. Gets or sets a value indicating whether the form adjusts its size to fit the height of the font used on the form and scales its controls. (Inherited from Form) | |
| AutoScaleBaseSize | Gets or sets the base size used for autoscaling of the form. (Inherited from Form) | |
| AutoScaleDimensions | Gets or sets the dimensions that the control was designed to. (Inherited from ContainerControl) | |
| AutoScaleMode | Gets or sets the automatic scaling mode of the control. (Inherited from ContainerControl) | |
| AutoScroll | Gets or sets a value indicating whether the form enables autoscrolling. (Inherited from Form) | |
| AutoScrollMargin | Gets or sets the size of the auto-scroll margin. (Inherited from ScrollableControl) | |
| AutoScrollMinSize | Gets or sets the minimum size of the auto-scroll. (Inherited from ScrollableControl) | |
| AutoScrollOffset | Gets or sets where this control is scrolled to in ScrollControlIntoView(Control). (Inherited from Control) | |
| AutoScrollPosition | Gets or sets the location of the auto-scroll position. (Inherited from ScrollableControl) | |
| AutoSize | Resize the form according to the setting of AutoSizeMode. (Inherited from Form) | |
| AutoSizeMode | Gets or sets the mode by which the form automatically resizes itself. (Inherited from Form) | |
| AutoValidate | Gets or sets a value that indicates whether controls in this container will be automatically validated when the focus changes. (Inherited from Form) | |
| BackColor | Gets or sets the background color for the control. (Inherited from Form) | |
| BackgroundImage | Gets or sets the background image displayed in the control. (Inherited from Control) | |
| BackgroundImageLayout | Gets or sets the background image layout as defined in the ImageLayout enumeration. (Inherited from Control) | |
| BindingContext | Gets or sets the BindingContext for the control. (Inherited from ContainerControl) | |
| Bottom | Gets the distance, in pixels, between the bottom edge of the control and the top edge of its container's client area. (Inherited from Control) | |
| Bounds | Gets or sets the size and location of the control including its nonclient elements, in pixels, relative to the parent control. (Inherited from Control) | |
| CancelButton | Gets or sets the button control that is clicked when the user presses the ESC key. (Inherited from Form) | |
| CanFocus | Gets a value indicating whether the control can receive focus. (Inherited from Control) | |
| CanSelect | Gets a value indicating whether the control can be selected. (Inherited from Control) | |
| Capture | Gets or sets a value indicating whether the control has captured the mouse. (Inherited from Control) | |
| CausesValidation | Gets or sets a value indicating whether the control causes validation to be performed on any controls that require validation when it receives focus. (Inherited from Control) | |
| ClientRectangle | Gets the rectangle that represents the client area of the control. (Inherited from Control) | |
| ClientSize | Gets or sets the size of the client area of the form. (Inherited from Form) | |
| CompanyName | Gets the name of the company or creator of the application containing the control. (Inherited from Control) | |
| Container | Gets the IContainer that contains the Component. (Inherited from Component) | |
| ContainsFocus | Gets a value indicating whether the control, or one of its child controls, currently has the input focus. (Inherited from Control) | |
| ContextMenu | Gets or sets the shortcut menu associated with the control. (Inherited from Control) | |
| ContextMenuStrip | Gets or sets the ContextMenuStrip associated with this control. (Inherited from Control) | |
| ControlBox | Gets or sets a value indicating whether a control box is displayed in the caption bar of the form. (Inherited from Form) | |
| Controls | Gets the collection of controls contained within the control. (Inherited from Control) | |
| Created | Gets a value indicating whether the control has been created. (Inherited from Control) | |
| CurrentAutoScaleDimensions | Gets the current run-time dimensions of the screen. (Inherited from ContainerControl) | |
| Cursor | Gets or sets the cursor that is displayed when the mouse pointer is over the control. (Inherited from Control) | |
| DataBindings | Gets the data bindings for the control. (Inherited from Control) | |
| DesktopBounds | Gets or sets the size and location of the form on the Windows desktop. (Inherited from Form) | |
| DesktopLocation | Gets or sets the location of the form on the Windows desktop. (Inherited from Form) | |
| DeviceDpi | Gets the DPI value for the display device where the control is currently being displayed. (Inherited from Control) | |
| DialogResult | Gets or sets the dialog result for the form. (Inherited from Form) | |
| DisplayRectangle | Gets the rectangle that represents the virtual display area of the control. (Inherited from ScrollableControl) | |
| Disposing | Gets a value indicating whether the base Control class is in the process of disposing. (Inherited from Control) | |
| Dock | Gets or sets which control borders are docked to its parent control and determines how a control is resized with its parent. (Inherited from Control) | |
| DockPadding | Gets the dock padding settings for all edges of the control. (Inherited from ScrollableControl) | |
| Enabled | Gets or sets a value indicating whether the control can respond to user interaction. (Inherited from Control) | |
| Focused | Gets a value indicating whether the control has input focus. (Inherited from Control) | |
| Font | Gets or sets the font of the text displayed by the control. (Inherited from Control) | |
| ForeColor | Gets or sets the foreground color of the control. (Inherited from Control) | |
| FormBorderStyle | Gets or sets the border style of the form. (Inherited from Form) | |
| Handle | Gets the window handle that the control is bound to. (Inherited from Control) | |
| HasChildren | Gets a value indicating whether the control contains one or more child controls. (Inherited from Control) | |
| Height | Gets or sets the height of the control. (Inherited from Control) | |
| HelpButton | Gets or sets a value indicating whether a Help button should be displayed in the caption box of the form. (Inherited from Form) | |
| HorizontalScroll | Gets the characteristics associated with the horizontal scroll bar. (Inherited from ScrollableControl) | |
| Icon | Gets or sets the icon for the form. (Inherited from Form) | |
| ImeMode | Gets or sets the Input Method Editor (IME) mode of the control. (Inherited from Control) | |
| InvokeRequired | Gets a value indicating whether the caller must call an invoke method when making method calls to the control because the caller is on a different thread than the one the control was created on. (Inherited from Control) | |
| IsAccessible | Gets or sets a value indicating whether the control is visible to accessibility applications. (Inherited from Control) | |
| IsDisposed | Gets a value indicating whether the control has been disposed of. (Inherited from Control) | |
| IsHandleCreated | Gets a value indicating whether the control has a handle associated with it. (Inherited from Control) | |
| IsMdiChild | Gets a value indicating whether the form is a multiple-document interface (MDI) child form. (Inherited from Form) | |
| IsMdiContainer | Gets or sets a value indicating whether the form is a container for multiple-document interface (MDI) child forms. (Inherited from Form) | |
| IsMirrored | Gets a value indicating whether the control is mirrored. (Inherited from Control) | |
| IsRestrictedWindow | Gets a value indicating whether the form can use all windows and user input events without restriction. (Inherited from Form) | |
| KeyPreview | Gets or sets a value indicating whether the form will receive key events before the event is passed to the control that has focus. (Inherited from Form) | |
| LayoutEngine | Gets a cached instance of the control's layout engine. (Inherited from Control) | |
| Left | Gets or sets the distance, in pixels, between the left edge of the control and the left edge of its container's client area. (Inherited from Control) | |
| Location | Gets or sets the Point that represents the upper-left corner of the Form in screen coordinates. (Inherited from Form) | |
| MainMenuStrip | Gets or sets the primary menu container for the form. (Inherited from Form) | |
| Margin | Gets or sets the space between controls. (Inherited from Form) | |
| MaximizeBox | Gets or sets a value indicating whether the Maximize button is displayed in the caption bar of the form. (Inherited from Form) | |
| MaximumSize | Gets the maximum size the form can be resized to. (Inherited from Form) | |
| MdiChildren | Gets an array of forms that represent the multiple-document interface (MDI) child forms that are parented to this form. (Inherited from Form) | |
| MdiParent | Gets or sets the current multiple-document interface (MDI) parent form of this form. (Inherited from Form) | |
| Menu | Gets or sets the MainMenu that is displayed in the form. (Inherited from Form) | |
| MergedMenu | Gets the merged menu for the form. (Inherited from Form) | |
| MinimizeBox | Gets or sets a value indicating whether the Minimize button is displayed in the caption bar of the form. (Inherited from Form) | |
| MinimumSize | Gets or sets the minimum size the form can be resized to. (Inherited from Form) | |
| Modal | Gets a value indicating whether this form is displayed modally. (Inherited from Form) | |
| Name | Gets or sets the name of the control. (Inherited from Control) | |
| Opacity | Gets or sets the opacity level of the form. (Inherited from Form) | |
| OwnedForms | Gets an array of Form objects that represent all forms that are owned by this form. (Inherited from Form) | |
| Owner | Gets or sets the form that owns this form. (Inherited from Form) | |
| Padding | Gets or sets padding within the control. (Inherited from Control) | |
| Parent | Gets or sets the parent container of the control. (Inherited from Control) | |
| ParentForm | Gets the form that the container control is assigned to. (Inherited from ContainerControl) | |
| PreferredSize | Gets the size of a rectangular area into which the control can fit. (Inherited from Control) | |
| ProductName | Gets the product name of the assembly containing the control. (Inherited from Control) | |
| ProductVersion | Gets the version of the assembly containing the control. (Inherited from Control) | |
| RecreatingHandle | Gets a value indicating whether the control is currently re-creating its handle. (Inherited from Control) | |
| Region | Gets or sets the window region associated with the control. (Inherited from Control) | |
| RestoreBounds | Gets the location and size of the form in its normal window state. (Inherited from Form) | |
| ReturnValue | ||
| Right | Gets the distance, in pixels, between the right edge of the control and the left edge of its container's client area. (Inherited from Control) | |
| RightToLeft | Gets or sets a value indicating whether control's elements are aligned to support locales using right-to-left fonts. (Inherited from Control) | |
| RightToLeftLayout | Gets or sets a value indicating whether right-to-left mirror placement is turned on. (Inherited from Form) | |
| ShowIcon | Gets or sets a value indicating whether an icon is displayed in the caption bar of the form. (Inherited from Form) | |
| ShowInTaskbar | Gets or sets a value indicating whether the form is displayed in the Windows taskbar. (Inherited from Form) | |
| Site | Gets or sets the site of the control. (Inherited from Control) | |
| Size | Gets or sets the size of the form. (Inherited from Form) | |
| SizeGripStyle | Gets or sets the style of the size grip to display in the lower-right corner of the form. (Inherited from Form) | |
| StartPosition | Gets or sets the starting position of the form at run time. (Inherited from Form) | |
| TabIndex | Gets or sets the tab order of the control within its container. (Inherited from Form) | |
| TabStop | Gets or sets a value indicating whether the user can give the focus to this control using the TAB key. (Inherited from Form) | |
| Tag | Gets or sets the object that contains data about the control. (Inherited from Control) | |
| Text | Gets or sets the text associated with this control. (Inherited from Form) | |
| Top | Gets or sets the distance, in pixels, between the top edge of the control and the top edge of its container's client area. (Inherited from Control) | |
| TopLevel | Gets or sets a value indicating whether to display the form as a top-level window. (Inherited from Form) | |
| TopLevelControl | Gets the parent control that is not parented by another Windows Forms control. Typically, this is the outermost Form that the control is contained in. (Inherited from Control) | |
| TopMost | Gets or sets a value indicating whether the form should be displayed as a topmost form. (Inherited from Form) | |
| TransparencyKey | Gets or sets the color that will represent transparent areas of the form. (Inherited from Form) | |
| UseWaitCursor | Gets or sets a value indicating whether to use the wait cursor for the current control and all child controls. (Inherited from Control) | |
| VerticalScroll | Gets the characteristics associated with the vertical scroll bar. (Inherited from ScrollableControl) | |
| Visible | Gets or sets a value indicating whether the control and all its child controls are displayed. (Inherited from Control) | |
| Width | Gets or sets the width of the control. (Inherited from Control) | |
| WindowState | Gets or sets a value that indicates whether form is minimized, maximized, or normal. (Inherited from Form) | |
| WindowTarget | This property is not relevant for this class. (Inherited from Control) |
| Name | Description | |
|---|---|---|
| Activate | Activates the form and gives it focus. (Inherited from Form) | |
| AddOwnedForm | Adds an owned form to this form. (Inherited from Form) | |
| BeginInvoke(Delegate) | Executes the specified delegate asynchronously on the thread that the control's underlying handle was created on. (Inherited from Control) | |
| BeginInvoke(Delegate, Object) | Executes the specified delegate asynchronously with the specified arguments, on the thread that the control's underlying handle was created on. (Inherited from Control) | |
| BringToFront | Brings the control to the front of the z-order. (Inherited from Control) | |
| Close | Closes the form. (Inherited from Form) | |
| Contains | Retrieves a value indicating whether the specified control is a child of the control. (Inherited from Control) | |
| CreateControl | Forces the creation of the visible control, including the creation of the handle and any visible child controls. (Inherited from Control) | |
| CreateGraphics | Creates the Graphics for the control. (Inherited from Control) | |
| CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from MarshalByRefObject) | |
| Dispose | Releases all resources used by the Component. (Inherited from Component) | |
| DoDragDrop | Begins a drag-and-drop operation. (Inherited from Control) | |
| DrawToBitmap | Supports rendering to the specified bitmap. (Inherited from Control) | |
| EndInvoke | Retrieves the return value of the asynchronous operation represented by the IAsyncResult passed. (Inherited from Control) | |
| Equals | Determines whether the specified object is equal to the current object. (Inherited from Object) | |
| FindForm | Retrieves the form that the control is on. (Inherited from Control) | |
| Focus | Sets input focus to the control. (Inherited from Control) | |
| GetChildAtPoint(Point) | Retrieves the child control that is located at the specified coordinates. (Inherited from Control) | |
| GetChildAtPoint(Point, GetChildAtPointSkip) | Retrieves the child control that is located at the specified coordinates, specifying whether to ignore child controls of a certain type. (Inherited from Control) | |
| GetContainerControl | Returns the next ContainerControl up the control's chain of parent controls. (Inherited from Control) | |
| GetHashCode | Serves as the default hash function. (Inherited from Object) | |
| GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from MarshalByRefObject) | |
| GetNextControl | Retrieves the next control forward or back in the tab order of child controls. (Inherited from Control) | |
| GetPreferredSize | Retrieves the size of a rectangular area into which a control can be fitted. (Inherited from Control) | |
| GetType | Gets the Type of the current instance. (Inherited from Object) | |
| Hide | Conceals the control from the user. (Inherited from Control) | |
| InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from MarshalByRefObject) | |
| Invalidate | Invalidates the entire surface of the control and causes the control to be redrawn. (Inherited from Control) | |
| Invalidate(Boolean) | Invalidates a specific region of the control and causes a paint message to be sent to the control. Optionally, invalidates the child controls assigned to the control. (Inherited from Control) | |
| Invalidate(Rectangle) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. (Inherited from Control) | |
| Invalidate(Region) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. (Inherited from Control) | |
| Invalidate(Rectangle, Boolean) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. Optionally, invalidates the child controls assigned to the control. (Inherited from Control) | |
| Invalidate(Region, Boolean) | Invalidates the specified region of the control (adds it to the control's update region, which is the area that will be repainted at the next paint operation), and causes a paint message to be sent to the control. Optionally, invalidates the child controls assigned to the control. (Inherited from Control) | |
| Invoke(Delegate) | Executes the specified delegate on the thread that owns the control's underlying window handle. (Inherited from Control) | |
| Invoke(Delegate, Object) | Executes the specified delegate, on the thread that owns the control's underlying window handle, with the specified list of arguments. (Inherited from Control) | |
| LayoutMdi | Arranges the multiple-document interface (MDI) child forms within the MDI parent form. (Inherited from Form) | |
| LogicalToDeviceUnits | Converts a Logical DPI value to it's equivalent DeviceUnit DPI value. (Inherited from Control) | |
| PerformAutoScale | Performs scaling of the container control and its children. (Inherited from ContainerControl) | |
| PerformLayout | Forces the control to apply layout logic to all its child controls. (Inherited from Control) | |
| PerformLayout(Control, String) | Forces the control to apply layout logic to all its child controls. (Inherited from Control) | |
| PointToClient | Computes the location of the specified screen point into client coordinates. (Inherited from Control) | |
| PointToScreen | Computes the location of the specified client point into screen coordinates. (Inherited from Control) | |
| PreProcessControlMessage | Preprocesses keyboard or input messages within the message loop before they are dispatched. (Inherited from Control) | |
| PreProcessMessage | Preprocesses keyboard or input messages within the message loop before they are dispatched. (Inherited from Control) | |
| RectangleToClient | Computes the size and location of the specified screen rectangle in client coordinates. (Inherited from Control) | |
| RectangleToScreen | Computes the size and location of the specified client rectangle in screen coordinates. (Inherited from Control) | |
| Refresh | Forces the control to invalidate its client area and immediately redraw itself and any child controls. (Inherited from Control) | |
| RemoveOwnedForm | Removes an owned form from this form. (Inherited from Form) | |
| ResetBackColor | Resets the BackColor property to its default value. (Inherited from Control) | |
| ResetBindings | Causes a control bound to the BindingSource to reread all the items in the list and refresh their displayed values. (Inherited from Control) | |
| ResetCursor | Resets the Cursor property to its default value. (Inherited from Control) | |
| ResetFont | Resets the Font property to its default value. (Inherited from Control) | |
| ResetForeColor | Resets the ForeColor property to its default value. (Inherited from Control) | |
| ResetImeMode | Resets the ImeMode property to its default value. (Inherited from Control) | |
| ResetRightToLeft | Resets the RightToLeft property to its default value. (Inherited from Control) | |
| ResetText | Resets the Text property to its default value. (Inherited from Control) | |
| ResumeLayout | Resumes usual layout logic. (Inherited from Control) | |
| ResumeLayout(Boolean) | Resumes usual layout logic, optionally forcing an immediate layout of pending layout requests. (Inherited from Control) | |
| Scale(Single) | Obsolete. Scales the control and any child controls. (Inherited from Control) | |
| Scale(SizeF) | Scales the control and all child controls by the specified scaling factor. (Inherited from Control) | |
| Scale(Single, Single) | Obsolete. Scales the entire control and any child controls. (Inherited from Control) | |
| ScaleBitmapLogicalToDevice | Scales a logical bitmap value to it's equivalent device unit value when a DPI change occurs. (Inherited from Control) | |
| ScrollControlIntoView | Scrolls the specified child control into view on an auto-scroll enabled control. (Inherited from ScrollableControl) | |
| Select | Activates the control. (Inherited from Control) | |
| SelectNextControl | Activates the next control. (Inherited from Control) | |
| SendToBack | Sends the control to the back of the z-order. (Inherited from Control) | |
| SetAutoScrollMargin | Sets the size of the auto-scroll margins. (Inherited from ScrollableControl) | |
| SetBounds(Int32, Int32, Int32, Int32) | Sets the bounds of the control to the specified location and size. (Inherited from Control) | |
| SetBounds(Int32, Int32, Int32, Int32, BoundsSpecified) | Sets the specified bounds of the control to the specified location and size. (Inherited from Control) | |
| SetDesktopBounds | Sets the bounds of the form in desktop coordinates. (Inherited from Form) | |
| SetDesktopLocation | Sets the location of the form in desktop coordinates. (Inherited from Form) | |
| Show | Displays the control to the user. (Inherited from Control) | |
| Show(IWin32Window) | Shows the form with the specified owner to the user. (Inherited from Form) | |
| Show(Object, String, String, cMessageBoxButtons, cMessageBoxIcon) | ||
| Show(Object, String, String, cMessageBoxButtons, cMessageBoxIcon, cMessageBoxDefaultButton) | ||
| Show(Object, String, String, String, cMessageBoxIcon, Int32) | ||
| Show(Object, String, String, String, cMessageBoxIcon, Int32, Int32) | ||
| ShowBox | ||
| ShowDialog | Shows the form as a modal dialog box. (Inherited from Form) | |
| ShowDialog(IWin32Window) | Shows the form as a modal dialog box with the specified owner. (Inherited from Form) | |
| SuspendLayout | Temporarily suspends the layout logic for the control. (Inherited from Control) | |
| ToString | Gets a string representing the current instance of the form. (Inherited from Form) | |
| Update | Causes the control to redraw the invalidated regions within its client area. (Inherited from Control) | |
| Validate | Verifies the value of the control losing focus by causing the Validating and Validated events to occur, in that order. (Inherited from ContainerControl) | |
| Validate(Boolean) | Verifies the value of the control that is losing focus; conditionally dependent on whether automatic validation is turned on. (Inherited from ContainerControl) | |
| ValidateChildren | Causes all of the child controls within a control that support validation to validate their data. (Inherited from Form) | |
| ValidateChildren(ValidationConstraints) | Causes all of the child controls within a control that support validation to validate their data. (Inherited from Form) |
| Name | Description | |
|---|---|---|
| Activated | Occurs when the form is activated in code or by the user. (Inherited from Form) | |
| AutoSizeChanged | Occurs when the AutoSize property changes. (Inherited from Form) | |
| AutoValidateChanged | Occurs when the AutoValidate property changes. (Inherited from Form) | |
| BackColorChanged | Occurs when the value of the BackColor property changes. (Inherited from Control) | |
| BackgroundImageChanged | Occurs when the value of the BackgroundImage property changes. (Inherited from Control) | |
| BackgroundImageLayoutChanged | Occurs when the BackgroundImageLayout property changes. (Inherited from Control) | |
| BindingContextChanged | Occurs when the value of the BindingContext property changes. (Inherited from Control) | |
| CausesValidationChanged | Occurs when the value of the CausesValidation property changes. (Inherited from Control) | |
| ChangeUICues | Occurs when the focus or keyboard user interface (UI) cues change. (Inherited from Control) | |
| Click | Occurs when the control is clicked. (Inherited from Control) | |
| ClientSizeChanged | Occurs when the value of the ClientSize property changes. (Inherited from Control) | |
| Closed | Occurs when the form is closed. (Inherited from Form) | |
| Closing | Occurs when the form is closing. (Inherited from Form) | |
| ContextMenuChanged | Occurs when the value of the ContextMenu property changes. (Inherited from Control) | |
| ContextMenuStripChanged | Occurs when the value of the ContextMenuStrip property changes. (Inherited from Control) | |
| ControlAdded | Occurs when a new control is added to the ControlControlCollection. (Inherited from Control) | |
| ControlRemoved | Occurs when a control is removed from the ControlControlCollection. (Inherited from Control) | |
| CursorChanged | Occurs when the value of the Cursor property changes. (Inherited from Control) | |
| Deactivate | Occurs when the form loses focus and is no longer the active form. (Inherited from Form) | |
| Disposed | Occurs when the component is disposed by a call to the Dispose method. (Inherited from Component) | |
| DockChanged | Occurs when the value of the Dock property changes. (Inherited from Control) | |
| DoubleClick | Occurs when the control is double-clicked. (Inherited from Control) | |
| DpiChanged | Occurs when the DPI setting changes on the display device where the form is currently displayed. (Inherited from Form) | |
| DpiChangedAfterParent | Occurs when the DPI setting for a control is changed programmatically after the DPI of its parent control or form has changed. (Inherited from Control) | |
| DpiChangedBeforeParent | Occurs when the DPI setting for a control is changed programmatically before a DPI change event for its parent control or form has occurred. (Inherited from Control) | |
| DragDrop | Occurs when a drag-and-drop operation is completed. (Inherited from Control) | |
| DragEnter | Occurs when an object is dragged into the control's bounds. (Inherited from Control) | |
| DragLeave | Occurs when an object is dragged out of the control's bounds. (Inherited from Control) | |
| DragOver | Occurs when an object is dragged over the control's bounds. (Inherited from Control) | |
| EnabledChanged | Occurs when the Enabled property value has changed. (Inherited from Control) | |
| Enter | Occurs when the control is entered. (Inherited from Control) | |
| FontChanged | Occurs when the Font property value changes. (Inherited from Control) | |
| ForeColorChanged | Occurs when the ForeColor property value changes. (Inherited from Control) | |
| FormClosed | Occurs after the form is closed. (Inherited from Form) | |
| FormClosing | Occurs before the form is closed. (Inherited from Form) | |
| GiveFeedback | Occurs during a drag operation. (Inherited from Control) | |
| GotFocus | Occurs when the control receives focus. (Inherited from Control) | |
| HandleCreated | Occurs when a handle is created for the control. (Inherited from Control) | |
| HandleDestroyed | Occurs when the control's handle is in the process of being destroyed. (Inherited from Control) | |
| HelpButtonClicked | Occurs when the Help button is clicked. (Inherited from Form) | |
| HelpRequested | Occurs when the user requests help for a control. (Inherited from Control) | |
| ImeModeChanged | Occurs when the ImeMode property has changed. (Inherited from Control) | |
| InputLanguageChanged | Occurs after the input language of the form has changed. (Inherited from Form) | |
| InputLanguageChanging | Occurs when the user attempts to change the input language for the form. (Inherited from Form) | |
| Invalidated | Occurs when a control's display requires redrawing. (Inherited from Control) | |
| KeyDown | Occurs when a key is pressed while the control has focus. (Inherited from Control) | |
| KeyPress | Occurs when a character. space or backspace key is pressed while the control has focus. (Inherited from Control) | |
| KeyUp | Occurs when a key is released while the control has focus. (Inherited from Control) | |
| Layout | Occurs when a control should reposition its child controls. (Inherited from Control) | |
| Leave | Occurs when the input focus leaves the control. (Inherited from Control) | |
| Load | Occurs before a form is displayed for the first time. (Inherited from Form) | |
| LocationChanged | Occurs when the Location property value has changed. (Inherited from Control) | |
| LostFocus | Occurs when the control loses focus. (Inherited from Control) | |
| MarginChanged | Occurs when the Margin property changes. (Inherited from Form) | |
| MaximizedBoundsChanged | Occurs when the value of the MaximizedBounds property has changed. (Inherited from Form) | |
| MaximumSizeChanged | Occurs when the value of the MaximumSize property has changed. (Inherited from Form) | |
| MdiChildActivate | Occurs when a multiple-document interface (MDI) child form is activated or closed within an MDI application. (Inherited from Form) | |
| MenuComplete | Occurs when the menu of a form loses focus. (Inherited from Form) | |
| MenuStart | Occurs when the menu of a form receives focus. (Inherited from Form) | |
| MinimumSizeChanged | Occurs when the value of the MinimumSize property has changed. (Inherited from Form) | |
| MouseCaptureChanged | Occurs when the control loses mouse capture. (Inherited from Control) | |
| MouseClick | Occurs when the control is clicked by the mouse. (Inherited from Control) | |
| MouseDoubleClick | Occurs when the control is double clicked by the mouse. (Inherited from Control) | |
| MouseDown | Occurs when the mouse pointer is over the control and a mouse button is pressed. (Inherited from Control) | |
| MouseEnter | Occurs when the mouse pointer enters the control. (Inherited from Control) | |
| MouseHover | Occurs when the mouse pointer rests on the control. (Inherited from Control) | |
| MouseLeave | Occurs when the mouse pointer leaves the control. (Inherited from Control) | |
| MouseMove | Occurs when the mouse pointer is moved over the control. (Inherited from Control) | |
| MouseUp | Occurs when the mouse pointer is over the control and a mouse button is released. (Inherited from Control) | |
| MouseWheel | Occurs when the mouse wheel moves while the control has focus. (Inherited from Control) | |
| Move | Occurs when the control is moved. (Inherited from Control) | |
| PaddingChanged | Occurs when the control's padding changes. (Inherited from Control) | |
| Paint | Occurs when the control is redrawn. (Inherited from Control) | |
| ParentChanged | Occurs when the Parent property value changes. (Inherited from Control) | |
| PreviewKeyDown | Occurs before the KeyDown event when a key is pressed while focus is on this control. (Inherited from Control) | |
| QueryAccessibilityHelp | Occurs when AccessibleObject is providing help to accessibility applications. (Inherited from Control) | |
| QueryContinueDrag | Occurs during a drag-and-drop operation and enables the drag source to determine whether the drag-and-drop operation should be canceled. (Inherited from Control) | |
| RegionChanged | Occurs when the value of the Region property changes. (Inherited from Control) | |
| Resize | Occurs when the control is resized. (Inherited from Control) | |
| ResizeBegin | Occurs when a form enters resizing mode. (Inherited from Form) | |
| ResizeEnd | Occurs when a form exits resizing mode. (Inherited from Form) | |
| RightToLeftChanged | Occurs when the RightToLeft property value changes. (Inherited from Control) | |
| RightToLeftLayoutChanged | Occurs after the value of the RightToLeftLayout property changes. (Inherited from Form) | |
| Scroll | Occurs when the user or code scrolls through the client area. (Inherited from ScrollableControl) | |
| Shown | Occurs whenever the form is first displayed. (Inherited from Form) | |
| SizeChanged | Occurs when the Size property value changes. (Inherited from Control) | |
| StyleChanged | Occurs when the control style changes. (Inherited from Control) | |
| SystemColorsChanged | Occurs when the system colors change. (Inherited from Control) | |
| TabIndexChanged | Occurs when the value of the TabIndex property changes. (Inherited from Form) | |
| TabStopChanged | Occurs when the TabStop property changes. (Inherited from Form) | |
| TextChanged | Occurs when the Text property value changes. (Inherited from Control) | |
| Validated | Occurs when the control is finished validating. (Inherited from Control) | |
| Validating | Occurs when the control is validating. (Inherited from Control) | |
| VisibleChanged | Occurs when the Visible property value changes. (Inherited from Control) |
| Name | Description | |
|---|---|---|
| UseConsoleMessageBox |